Q1: The internal Vref is 0.7V (used for SS/TR) typical, right?
Q2: I understand SS/TR is connected to a Current Source, which is connected to a mid-rail that comes from VIN - yes?
I am being asked for a high-level visual description...the functional block diagram in the DS doesn't quite have enough info to help gauge what the cap might see.
Q3: Could the cap connected to SS/TR pin see a voltage as high as VIN?
This information is needed to select the voltage rating of the SS/TR capacitor - I need to know the max voltage this pin could see.
Q4: Will forcibly bringing SS/TR pin to 0V cause the PGOOD signal to go LOW?
For reference, pulling the EN signal "Low" pulls PGOOD "Low", even before the output voltage has fallen.
Would bringing SS/TR to 0V also do the same thing?