Other Parts Discussed in Thread: CSD16342Q5A, LM25145, LM3150, LM25149, LM25148, LM5146, LM5145, LM63460-Q1
Hi TI,
I'm going to use this convertor in my PCB board for below mentioned configuration,
Vin = 12 V to 20 V
Iout = 6A
Vout = 5 V
Ambient temperature = 90 degree celsius
using CSD16342Q5A FET (webench suggested part) , In Evaluation Board application note AN-1900 (SNVA371) for PCB design there it has PCB layout for placing FET,
my query is if I follow the layout whether it achieve FCC class B radiation emission testing ?.