This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS566231: Distribution of Soft Start Time

Part Number: TPS566231

Hello,

Can you share the distribution of soft start time.  I see the max of 2.9ms which violates a use case condition in my design. I need to keep soft start under 2.5ms.  When I review Figure 6-16 at the 12Vin use case , the soft start does not change over temperature.  Are there other factors that are affecting this 2.9ms max?

Thanks,

Jason

  • Hi Jason,

    Sorry, we don't have distribution of soft start data for TPS566231P. Please refer to typ./min./max values as listed in datasheet. There is no other factor that affects this 2.9ms max and it is just part to part variation. If you need a fast soft start time, you can use TPS566231 which has programmable soft start with a cap.

    Thanks,

    Nancy