This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5046: Phase-Shifted Full-Bridge PWM Controller

Part Number: LM5046


I have been tasked with creating a 208/120 VAC 3 Phase. SMPS with an output of 270VDC, 60A, 16kW 

I will have a 270V Bus Generated by 11 SynQor MPFC-115-3PH-270-FP 3 Phase  1.5kW PFC Modules operating in Parallel and will use a LM5046 - Phase-Shifted Full-Bridge PWM Controller to regulated 270VDC output.  I am considering using 5 in parallel that would mean 12A each, is this practical