Question about "Fusion Digital Power Designer" (aka FDPD) - no access to "Export" function
Details:
Have FDPD version 7.7.1 installed, USB Adapter attached (firmware rev 1.0.11) but UCD90xx device is NOT connected (I have no sample of UCD90xx device yet)
I've run FDPD in "Offline mode" and created/defined simple System based on UCD90160A
Problem: Can not figure out how to Export system (aka device configuration into neither flash file nor PMBus command script).
The documentation "8524.Configuration Programming of UCD Devices.pdf" says " 4.1 Export Using the Fusion GUI The Fusion GUI is normally used to export device configuration data. To begin, you select Export from the File menu:" But I can't find any "Export" sub/menu anywhere in the app.
Question: Does FDPD support export in "Offline mode"? If yes then how to access it?