Hi,
I have created a model based on TPS2597X_TRANS.lib. When I try to do a transient analysis, I get the error
"Cant find definition of model "DBREAK".
When I look into the LIB file I can see this is a diode in
D_U4_D12 U4_N01176 IN Dbreak
Also I get a bunch or errors after the simulation like
"Questionable use of curly braces in "b§e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}"
Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))"
Questionable use of curly braces in "b§e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}"
Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))"
Questionable use of curly braces in "b§e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}"
Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))"
Questionable use of curly braces in "b§e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}"
Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))"
..."
Complete log file attached here.
Circuit: * C:\Baraja\YOFC EDFA Testing\SIMs\TPS2597.asc Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}}&v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh))&v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}}|v(d)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh))|v(d)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(s)>{{vthresh}},v(b),v(a))}" Error: undefined symbol in: "if([v](s)>((vthresh)),v(b),v(a))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}}&v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh))&v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}}&v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh))&v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(s)>{{vthresh}},v(b),v(a))}" Error: undefined symbol in: "if([v](s)>((vthresh)),v(b),v(a))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(s)>{{vthresh}},v(b),v(a))}" Error: undefined symbol in: "if([v](s)>((vthresh)),v(b),v(a))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}}|v(c)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh))|v(c)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate1 yint1 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate2 yint3 0 v={if(v(yint2)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](yint2)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}|v(b)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh))|v(b)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vss}},{{vdd}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vss)),((vdd)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}}&v(b)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh))&v(b)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Questionable use of curly braces in "b�e_abmgate yint 0 v={if(v(a)>{{vthresh}},{{vdd}},{{vss}})}" Error: undefined symbol in: "if([v](a)>((vthresh)),((vdd)),((vss)))" Error on line 116 : d:u1:_u4_d12 u1:u4_n01176 vin�:in� dbreak Unable to find definition of model "dbreak" WARNING: Less than two connections to node U1:1V_DC. This node is used by V:U1:_V1. Direct Newton iteration for .op point skipped. Gmin stepping method for .op point skipped. Starting source stepping with srcstepmethod=0 Source Step = 3.0303% Source Step = 33.3333% Source Step = 63.6364% Source Step = 93.9394% Source stepping succeeded in finding the operating point. Ignoring empty pin current: Ix(u1:en_uvlo) Ignoring empty pin current: Ix(u1:en_uvlo) Date: Tue Feb 08 16:57:22 2022 Total elapsed time: 219.049 seconds. tnom = 27 temp = 27 method = Gear totiter = 2824 traniter = 2664 tranpoints = 1319 accept = 1278 rejected = 41 matrix size = 1192 fillins = 694 solver = Alternate Thread vector: 415.0/105.9[8] 73.7/35.0[8] 252.8/65.5[8] 12.7/15.0[1] 2592/500 Matrix Compiler1: 77.48 KB object code size 93.4/44.1/[22.0] Matrix Compiler2: 96.37 KB object code size 60.0/51.0/[17.6]
How can I solve these two issues?
Cheers,
Kaushalya