I have a question about the default values of the following registers on reset...
「VOUT_COMMAND」
「VOUT_MARGIN_HIGH」
「VOUT_MARGIN_LO」
The lower 10-bits are set by the pin-strap on boot/initializaiton.
I understand that the initial boot voltage starts up with the last saved NVM configuration of VOUT_COMMAND if the pin strap is either Open, 187 kΩ, 1.78 kΩ, or 0 Ω (short); otherwise the pin strap resistor RVSEL takes precedence.
But what about in the default state where NVM has yet to have any value stored to it?
What are the 10-bits in these registers then?
Regards,
Darren