This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A84A: Clarification with figures on the datasheet

Part Number: TPS7A84A

Hi Team,

A customer found a discrepancy with the datasheet for TPS7A84A. 

The customer pointed out that Figure 6-8 shows 60dB PSRR for 10Hz to 10MHz bandwidth, at Vin = 1.3V, Vout = 1V, Iout = 3A

However, these results appear to contradict Figure 6-5.

what should the customer do for only adding Cout 47uF,10uF,10uF with VBIAS?

Figure 6-5 and 6-8 have almost same test conditions but have very different PSRR result

Which is correct?

Hoping you can help.

Regards,

Marvin