Hi,
Based on 9.2.2.4 Inductor Selection in LMR33610 datasheet, the inductor value I calculated is 33uH. But we are using 15uH in the current circuit. Will there be any problem with lower inductor value?
Besides, I also consider to use LMR33630ADDA to replace LMR33610ADDAR. And the calculated value is 11uH based on the formula. If LMR33630ADDA is used instead of LMR33610ADDAR, is it appropriate to use the 15uH for this inductor?
Thanks!
Best regards,
Tianze