Other Parts Discussed in Thread: SN6505B, UCC14240-Q1, UCC25800
Hi Team,
Can you please advise with following request?
"
I was interested in this product because it can drive a 600V switch. I need a half bridge driver that can drive over 200V. However, I had to give up because I realized that it could not work at 100% duty cycle since the bootstrap structure was used in the product. I plan to continue with the product of a different company. In our application, switching will be made in the range of 200V-0V and it should be able to operate in the frequency range of DC to 10kHz. It is important to provide DC voltage (100% duty cycle) indefinitely. If you have such a product, I would like to review it.
However, if there is a chip with dead-time feature, it will be superior to the product of the other company I mentioned. dead-time can be configurable or if it is fixed, it should be <1us.
"
Thanks in advance
Best Regards
Furkan Sefiloglu