This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2026: Using BQStudio and EV2400 to communicate with device

Part Number: BQ2026
Other Parts Discussed in Thread: BQSTUDIO, , BQ2024, EV2400

Hello,

How would you use BQStudio and the EV2400 to communicate over HDQ interface to the BQ2022, BQ2024 or BQ2026 devices? 

When I start the program while the programmer is plugged to USB and the BQ2024 is plugged to HDQ, I see the following message:

I select All and then I see:

In the list, I do not see options for any of the BQ2022, BQ2024 and BQ2026 devices. Picking the first device in the list, looking around in the program, I don't see anywhere to read the content of the connected EPROM or be able to write a hex file into that.

Thanks,

John