Part Number: LM3424

hello sir i am trying to understand the internal block diagram of LM3424 I got stuck in loop compensation part where i couldn't understand the symbol being used in block diagram which i have marked separately in the screenshot of block diagram attached with this post .
as per my understanding i assumed it as tristate buffer and considered the output from ndim comparator as control pin of the tristate buffer and input and output of tristate buffer as output from HSP/HSN comparator and comp pin respectively
assuming the above thing correct i setup the LM3424 as buck without dimming (i.e ndim tied to voltage above 1.24 using potential divider circuit to act as UVLO) and tried to check voltages at pin of LM3424 what i observed was that i couldn't run my LED and the COMP pin was having voltage around 0.2volt only which i didn't expected as CSH was around 0.1volt forcing comparator at CSH to output +5volt and thereby forcing COMP at +5V
please help in understanding of this symbol used in block diagram