Hi team,
I would like to ask all device with "Power Path" feature can enable that system is powered by battery or adapter? Or only devices with PMID can do?
Let me explain a situation.
There is 12V adapter input and 2 cell battery to be charged. And system requires 10V. When adapter is plugged, The adapter charges battery and supply the current to the 10V system, on the other hands, the adapter is not plugged, the battery supply to 10V.
In this case, what is the recommendation of battery charger? Are all chargers with Power Path able to do? Does the system require buck-boost to generate 10V from both 12V or 6V-8.2V?
Best regards,
Hideki