Part Number: LM2941
Hi Team,
Our customer built some products using LM2941SX/NOPB. Some devices are not producing the expected output and thus the customer has to make adjustments to the design of the boards that were failing to make the circuit provide the desired output voltage of 12V. Here are the output voltage of the good and failed devices.
U10- Pin 5 (Failing unit) voltage range adjusted by R241 11.10V – 11.87V
U10- Pin 5 (Passing Unit) Voltage range adjusted by R241 11.67 – 11.98
Please see attached schematic diagram.

The output voltage error seems to be due to the potentiometer R241. Can you please confirm?
Regards,
Danilo