Other Parts Discussed in Thread: UCC2891, UCC2892, UCC2893, UCC2894, UCC2897A
Hi E2E
When customers use LM5026 and refer to datasheet 8.2 and Figure 31, if they encounter problems with UVLO, please help to confirm and eliminate them.
As shown in the figure below:
Ch1: LM5026 VIN pin
Ch2: LM5026 UVLO pin
Ch3: LM5026 OUTA
Ch4: VDS of LM5026 OUTA Mosfet
According to the LM5026 datasheet 8.2, when the UVLO pin is less than 1.25V, the IC will shut down. But the following Ch2 is lower than 1.25V, the OUTA pin still continues to output signal.
1. LM5026 spec why OUTA pin still output signal when UVLO pin is less than 1.25V.
2. Can Vin be used as an ON/OFF signal? If you want to use the input voltage and protect it at 1.25V, please refer to Figure 27.
3. Description of MOSFET action mode in Standby mode between UVLO pin 0.4V~1.25V.
4. How to turn off OUTA and OUTB by controlling when the VIN voltage drops. Please provide suggested routes.
5. In addition, the Mosfet showed on the left as shown below, Q4B is P Mosfet, Q6B is N Mosfet. If you change Q4B to N Mosfet, is there any suggested route you can refer to?