Other Parts Discussed in Thread: BQ24170, BQ24172, BQ25616
Hi,
Good Day. Is BQ24170/BQ24172 is a good alternative to BQ24133. BQ24170 seems to be identical, function wise, to the BQ24133. Except that Charging Current is 4A instead of 2.5A. The only difference, on pin 14, is the FB for the BQ24172. Otherwise the BQ24170, pin 14 has the same function. What are the limitations? What are the changes needed for BQ24170/BQ24172 to be as exact as BQ24133. Thank you very much.
Best Regards,
Ray Vincent