Other Parts Discussed in Thread: LP8733, TPS65218
Will there be a revised datasheet for the TPS6521855? To say the current one (August 2021) is a bit of a mess is an understatement.
Firstly, the voltage outputs are confusing. Is DCDC4 really 2.5V now? Everywhere else in the datasheet, and in all the diagrams, it's still listed as 3.3V.
What is the default output of LDO1? Is it 3.3V as stated on the front page, or 1.8V as hinted in the Electrical Characteristics and stated in the diagram in 7.2.
What is the default resistor required for DC34SEL? If the device has been programmed for 1.8V and 2.5V, none of these are options in table 7.2.
What is the point of table 8-1? This is a device-specific requirement for a different PMIC. Please only use examples for the target part, namely the AM64x.
From the Appnote for the LP873364/TPS65218xx, where does the PGOOD from this device connect to? (If it's no needed, don't include it?)
On the other linked Appnote (Powering the AM64x with the LP8733xx) PGOOD looks like it's connected to the EN signal of the same device!
Thanks for any clarifications!