Other Parts Discussed in Thread: TPS62110, TPS62111, TPS62110-Q1,
Hi Team,
Two questions from a customer:
1. The EP version of TPS62110 supports a higher temp range than the standard and Q1 versions for which it has a higher feedback voltage tolerance. Does the EP version support the lower feedback voltage tolerance up to 85C as well like the lower cost versions?
EP
Q1
2. With the TPS62111Q (automotive), the material may be in ambient air and processed for 168h, after which it must be dried. Then the 168h start over again. For TPS62111 (Industrial), the material may be in the ambient air for 1 year until it has to be dried. This makes sense considering the higher temperature tolerance of the Q1 version. But then the EP version with even higher temp range than Q1 can be stored for 1 year again. Can you elaborate on this please?
Thank you,
Franz