Part Number: TPSM82810
Hi Team,
We have received this inquiry from our customer.
Looking through the datasheet of TPSM8281x (as well as other voltage converters), there is typically a recommended effective output capacitance range provided. For the TPSM8281x this range is 27uF (min) to 470uF (max). What is meant by or included in this effective output capacitance limit? Does this capacitance include all capacitive loads on the output voltage rail and subsequent secondary voltage rails?
For example:
TPSM8281x effective output capacitance = C2 + C3 + [C4*(3V)^2]/(5V)^2, is this correct?
C4 is scaled from the 3V to the 5V rail using the capacitor energy formula (E=CV^2). Is this a valid method to scale the output capacitance of a converter or LDO to the input side? Or should this scaling be done using the capacitor charge formula (Q=CV)?
Regards,
Danilo