This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BUF11704: Power supply range

Part Number: BUF11704
Other Parts Discussed in Thread: BUF07704, , BUF11705

Hi,

In the past, customers have considered BUF11704 as a temporary replacement for BUF07704, but are considering BUF11705 because it is out of stock.

Q1)
Do the BUF11704 and 11705 have any different performance besides the difference in maximum power supply voltage?

Looking at the DS, it looks almost the same.

Q2)

The power supply voltage range: 4.5V ~ is stated on the top page of the DS of BUF11704.
However, the recommended power supply voltage for the DS P2 is 7V ~.
which one is correct?

Best regards,

Hiroshi