Other Parts Discussed in Thread: BQ76940, MSP-TS430PT48, , EV2400
We are working on the msp-ts430PT48 communicate with BQ76940 EVM through external I2c.
1> BQ76940EVM is working with EV2400 on GUI
We can send and receive I2c data from the window gui app
2> msp-ts430PT48 can run sample code modified from msp430fr2335 launch pad.
3> we run the code from http://www.ti.com/product/BQ76940/toolssoftware and did pull up action from code
P4SEL0 |= BIT6 + BIT7;
P4SEL1 = 0;
P4OUT |= BIT6 + BIT7;
P4REN |= BIT6 + BIT7;
we did see the address send out and captured from the scope , however, we did not see ACK from the BQ79640 for the very first time.
and register show UCNACKIFG = 1. UCTXIFG0 =1
How could be the issue here, please advise
Thanks