Other Parts Discussed in Thread: BQ24296
Hi team,
Here's an issue from the customer may need your help:
BQ24296 is used for battery management. When the battery is almost full: "The actual battery voltage is around 4v-4..1v"
The device jumps between fast charging and charge termination Done2 states.
- The Stat pin outputs a 20-Hz frequency, and the PGn output is low.
- Int always generates an interrupt (frequency is also 20 Hz).
- The value of the 00-09 register is 32 1B 20 11 b0 8b 73 4b a4 00, where the REG08 value jumps between a4 and b4, and the REG09 value is always 0.
- The TS pin uses a fixed resistor (10k) to divide the voltage, which is approximately 2.45v.
Below is the circuit:
Could you help check this case? Thanks.
Best Regards,
Cherry