Other Parts Discussed in Thread: LMR33620
Hi all,
My first question is in general about the TI categorization and how to use this inside a safety project. There is the split into different levels of functional safety capabilities and I am not really sure about how to use this categorization inside a project. The additional documentation on your homepage answers this question not completely .
The window wdg TPS3850G33QDRCRQ1 is rated as functional safety capable. So my understanding is that this component can be used as wdg in a safety related systems. The question here is if there are special requirements which needs to be fulfilled?
Regarding LMR33620-Q1. This is a DC/DC converter with an internal power good mechanism and here is the question if this can be used as monitoring function of the output voltage equal to a voltage monitor or are there restrictions which are not fulfilled by this component. From my point of view is an component with an integrated safety mechanism a class II component according to the norm
Class III:
“the element has internal safety mechanisms which are relevant for the safety concept to control
or detect internal failures.” ISO26262-8:2018 13.4.1.1
This means in my opinion that the DC/DC Converter with an internal power good monitoring must be considered as a class III element as long as the power good is used as a safety mechanism. Is this correct or is there a different interpretation on TI side? This means that it is really unlikely for a company to use this power good in a safety application.
Or what is the recommendation from TI side?
Best regards,
Björn