Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5009: LM5009 current limit status

Part Number: LM5009

Dear TI expert,

We have an existing application for LM5009. Input voltage is about 75V(yellow curve) and output voltage is about 14V(blue curve). RCL is about 300K,RON is about 475K and 1mH inductor

In our application, most of time the output current of LM5009 is about 5mA. but we want to switch off or on an bitstable relay (12VDC). the load of this bistable relay is 54 ohm and 100ms  duration. 

This load maybe cause current limit and cause the output voltage drop, but this votlage drop can be accepted from our application, as shown in pic..

Is there any risk for such current limit application ?