Hi Team,
Can you clarify what the actual output power of this device is, please?
The Buck modules of the TPSM5601R5 have an output power of 18W in the data sheet at the top of the features.
The current rating is max.1.5A (Limit_1.9A) and the output voltage range is 1~6V.
I would need to know which of these is true. My guess is that it is 9.6W output, as with other modules in this series.
For the modules with output voltages up to 16V, the power rating would be O.K. as the maximum value for the module.
Possibly it is only a printing error or a faulty takeover from a data sheet of a 9.6W module.

Thank you,
Franz