Other Parts Discussed in Thread: BQ25980
Hello, I'm a company in Korea, and I designed a battery charging circuit using BQ25890.
The battery used a lithium-ion polymer battery and was designed with a battery capacity of 4.2 V/10000 mA.
I used a USB C-type charger.
Charger Voltage used +5V/2.6A, +9V1.65A.
In the circuit I made, when the battery is fully charged and the remaining battery volume falls below 2.7V when using the system, when I try to charge to connecting USB C-type charger. charging is not good from this point on.
Than Charging takes place only when connected to a circuit in another auxiliary battery.
If you control the battery power not to fall below 3.1V, it is well recharged.
The problem is when the battery is discharged and goes below 3.1V.
Of course, the battery itself is used with built-in overdischarge and overcharge circuits.
I don't know why it's not charging.
When the discharged battery is connected to another auxiliary battery circuit, charging starts immediately. Can you check if my circuit is well designed?
My email address is as follows.
minkle69@daum.net, minkle69@ntcsoft.net
My company website is http://www.nntc.co.kr
I need the help of your engineer.
I hope to hear good news from you.
In the BQ25890 IC, the parameter setting value was put in the register according to the battery specification after looking at the data sheet.
Of course, Raspberry is connecting with BQ25890 through I2C communication to read, write, and test the values of the internal register.
please help me Dear
I can also send you a circuit diagram that I designed if you need it.