Hi Team,
Our customer is asking for some clarification from the datasheet. Would you kindly help?
I just want to confirm, from what I understand from the datasheet, the LM4040xQ is characterized for operation over an ambient temperature range of –40°C to 125°C and should be the same with LM4040xI. Could you explain why is it showing a difference for minimum cathode current at 25 degree C spec? (highlighted below).
In addition, LM4040DxI and LM4040DxQ have the same package SOT23 (DBZ) therefore these devices can replace each other. Correct?
Thank you.
Regards,
Marvin