Part Number: UCC5870QDWJEVM-026
To whom it may concern,
I am using a TI UCC5870QDWJEVM-026 evaluation board, but I am having issues writing to the registers using the included EVM software.
I have set up the evaluation board in both regular and daisy chain SPI modes, but in both cases, it is very hit and miss when moving from Configuration 1 into Configuration 2 - it will often refuse to move to Configuration 2, with no explanation as to why.
Additionally, I am trying to manually configure the registers using the Register view when I can get the chips into Configuration 2 - I cannot seem to change them to a value other than 0x0080 in any of the registers when using SPI in daisy chained mode. This is when setting automatic writes to off, as well as on.
I am wondering whether this has something to do with how the board boots - when power is applied, no faults or warnings show on the evaluation board.
However, I am able to use an alternative microcontroller to configure the evaluation board over SPI perfectly.
Thank you for your help in advance, and please let me know if you require any more information,
Kind regards,
Finn Beckitt-Marshall