Hi,
as we know, [LLCHBFirmware-1.2] is used for EVM149 + EVM150,
when look at the DTC section of the code, there is something strange as follow:
FILE: init_loop_mux.c
Funtion: init_DTC(void)
Line 108~111
//Select DPWM0B to be controlled by DTC Phase A
LoopMuxRegs.DTCCTRL.bit.PWM_A_SEL = 5; <= should be 2?
//Select DPWM1B to be controlled by DTC Phase B
LoopMuxRegs.DTCCTRL.bit.PWM_B_SEL = 6;
it set the DPWM0B and DPWM1B for the secondery SR driving?
refer to the circuit of EVM150, shouldn't it be the DPWM1A and DPWM1B?
I am confused, would you please expain this?
thanks!
Xiaofeng Wu