This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5521: Enable pin circuit

Part Number: LP5521


Hi,

Can you please help with the following question regarding enable pin? I am quoting below:

In the data sheet I miss concrete information about the wiring, e.g. at the start of the system, when it must be expected that the control line from the microcontroller driving the EN pin can be high impedance. In the circuit of the evaluation board LP5521TMEV I don't see any precautions (like pull-down resistor) for this case.

Can I take this as a reference circuit, or should I consider using a pull-down?

Regards,

Gokhan