Hi,
In the Revision A (May 2021) datasheet, two values are specified for worst-case low level for the /EN input pin - in chapter 6.3 (recommended operating conditions) it is 0.25V - in chapter 6.5 (electrical characteristics) it is 0.15V. Just a typo, and if yes then what is the correct value - or is there more to it than that?
Cheers, Martin