Hello, I'm having trouble discerning something in a datasheet for the linear regulator TLV767-Q1.
Here is the datasheet:
The line I am confused about is on page 6.
In the Electrical Characteristics, it is the Line Regulation (ripple) information at the far right, stating 0.02 %/V
Here is the whole line copy/pasted:
ΔVOUT(ΔVIN) Line regulation(1) VOUT(NOM) +1.5 V ≤ VIN ≤ 16 V, IOUT = 10 mA 0.02 %/V
What exactly does 0.02 %/V result in, if we can state it in mV?
The Output voltage in my application is 9V. The input is 12V, give or take 10mV.
I am looking for a regulator with a ripple spec that exceeds [ 1.6mV TYPICAL / 32mV MAX ] since that seems to be the best standard achievable for XX7809's of all brands/variations.
So, does 0.02 %/V mean 9 X 1.0002? If so, that gives us a high point in AC ripple of 9.0018. That is 1.8mV MAX, which would be quite good.
Or, does 0.02 %/V mean 9 X 1.02? If so, that gives us a high point in AC ripple of 9.18. That's 180mV MAX, which would be quite poor.
So i'm thinking it must be 1.8mV MAX. Does that seem correct?
Thanks to anyone who can help to confirm this!