Hi
I am trying to design battery unit system with two AA cell with output current of 3.3V, I would like to know how to calculate output current with different vin(as battery discharge.)
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
I am trying to design battery unit system with two AA cell with output current of 3.3V, I would like to know how to calculate output current with different vin(as battery discharge.)
Thanks
Hi Amir,
First thing is to understand the current limit specification. As shown in EC table TPS61016 has minimum 1.07A switch current limit.

Then you need to check how much efficiency level TPS61016 can go and choose one typical value. Choose 85%

Then calculate the inductor current ripple, assume 33uH inductance. For Vin=1.8V, the ripple is about 58.5mA.

So the maximum output current can be calculated as below:
=Vin*(1.07-0.5*0.058)*0.85/3.3=0.268Vin
You can simplify the equation per different Vin yourself.
-Wenhao