Hi team,
Customer is going to use LM34936-Q1 with below Vin ripple condition.
Vin : 21V
Input ripple voltage : 600mVp-p
Ripple frequency : 400kHz
Is these ripple no problem to the device behavior?
Because Figure 8-1 in the datasheet uses RC Filter(10ohm + 0.1uF) to VIN pin.
So, I'm concerned about if there are some noise requirement on th VIN pin.
Please check if LM34936-Q1 is no problem on above the ripple in the input voltage.
Regards,
Saito