Part Number: UCC5870QDWJEVM-026
Hello,
I have been using the UCC5870-Q1 GUI software on my colleague's laptop, but as my colleague is away, I am trying to run the software on my work PC. However, when I try to run it on my PC via the Start menu, I get no response, as the application does not seem to load. However, when I run via PowerShell/command prompt, I get the following error:
PS C:\guicomposer\runtime\gcruntime.v7\UCC5870-Q1EVMGUI> ..\win32\TICloudAgentHostApp\node.exe app_server.js --browser=..\win32\node-webkit\nw.exe --cloudAgentDir=win32
C:\guicomposer\runtime\gcruntime.v7\UCC5870-Q1EVMGUI\app_server.js:24
let appDataPath = process.env['APPDATA'];
^^^^^^^^^^^
SyntaxError: Unexpected identifier
at Module._compile (module.js:439:25)
at Object.Module._extensions..js (module.js:474:10)
at Module.load (module.js:356:32)
at Function.Module._load (module.js:312:12)
at Function.Module.runMain (module.js:497:10)
at startup (node.js:119:16)
at node.js:906:3
I am just wondering if there is anything I can do to resolve this? I have version 4.1.0.0 of the runtime installed on my PC - do I need to update this?
Kind regards,
Finn