Other Parts Discussed in Thread: TPS55288, TPS552882
Context:
I am using a 25V/1.2A photovoltaic panel to charge a 12V lithium iron (LiFePO4) battery with the evaluation board as an intermediate circuit to regulate the voltage and current. I chose this model due to the fact that the voltage regulators currently available would hit the necessary voltage but only supply 1/4 of the available current to the battery. Also, many of the other available buck/boost converters have a long lead time to receive; pretty much next year.
Question:
It is my understanding that this board can be programmed to user specifications using a GUI, but every time the board is powered off the registers get set back to default. My question is, are there any pins that can be used to supply external power to keep the board on while still receiving a Vin to buck/boost? If so which pins are they?
As one might deduce, nighttime would be a major problem if the board is powered off as the registers would set back to default. Ultimately I'd like to see if I can keep this board powered on by a separate external supply while still using Vin to buck/boost and have my specified Vout so that I don't have to program it each time.