The TPS22964C datasheet states:
The device contains a low RDSON N-Channel MOSFET that can operate over an input voltage range of 1 V to 5.5 V and switch currents of up to 3 A.
I want to know if the device can operate off a 1[V] supply.
Usually there will be some ripple/accuracy causing supply voltage to drop below 1[V] slightly.
1) What is the minimum supply voltage the device could function at...? (Is there a margin of 10mV or 100mV, etc?
2) Is this "1V" minimum decided by an UVLO feature in the device?
I need to know how much design margin there is to the "1V" statement...
Thanks!
Regards,
Darren