Hi!
I would like to know if there need to be additional parts (Schottky diode?) if we expect that a secondary supply may apply voltage to OUT/SNS.
For example:
1] The TLV766 may have 12V IN with a fixed output of 3.3V.
2] The 12V supply may be removed, turning off the TLV766 completely.
3] A secondary supply may begin supplying on the 3.3V line.
Can such a condition damage the TLV766 if there is no additional circuitry on the OUT/SNS pins?
One concern is that in case of using a diode on the output, the drop would be too significant to use the fixed 3.3V version of the TLV766.
An adjustable TLV766 circuit would have to be used that accounts for the diode's voltage drop.
Thank you!