When LM63635-Q1 power(VIN) off, standby mode occur Vout switching and keep about 2.4V.
(External setting on Voff: 6.45V_typ)
Please see attached waveform below;
※ch4:Inductor current
Please let me know about two points below;
①What is the reason for Vout switching and keep 2.4V on standby mode?
Is these waveform abnormal, please let me know idea for improve point.
②Is there possibility to reason for low Cboot value?
LM63635-Q1's circuit information
・24Vin → 5Vout / 3A
Vout is adjustable setting, VSEL connecting 10kΩ
・Cin: 10μF ×2, 0.22μF
・Cin: 22μF ×3, L:2.2μH
・Cboot: 220nF / 50V (maybe decrease by DC bias)
・fsw: 2.1MHz
・FPWM mode
・External UVLO setting
Von: 10.34V_typ, Voff: 6.45V_typ
・/RESET is floating (unused)
Best regards,
Satoshi