Dear Sir or Madam,
I have a design with the "TPS2121RUX". The Power management regarding switching between battery and main supply (by a regulator) works fine. I use the inputs OV1 and OV2 to give the switch an output enable and use a high signal level by a controller.
When OV1 and OV2 are high. The supply at IN1 is disabled and on IN2 is connected a battery with 4V. I can see that there is still a current flow into IN2 with approx. 115µA. I want to reduce this current. Where/why is this flow coming from? Any ideas?
Regarding the datasheet the leakage current in this standby should be lower:
I use follow configuration. In blue to see the state where I have the 115µA:
Follow schematic I have:
Thanks beforehand for your efforts.
Best regards
Wolfgang Walter