Hello,
My customer wnats to use the TPS54623 with the following conditions.
- VIN = 13V~15.5V, VOUT = fixed 12V, IOUT = 1A
If the VIN voltage is linearly changed from 13V to 10.7V, will the output 12V also drop linearly like the input voltage?
If there is any output voltage change data for such input voltage change, please share it.
Thanks.
JH