We built a circuit for converting 12V to 24V using TPS61175. The schematic of the same can seen below.
When we are trying to load the converter with DC fan at 24V the input power supply is going to CC at 3V . But when converter is turned on no load and when we connect fan directly the output voltage drops to 20V and fan is running at low speed.
Kindly suggest us how to move forward
DC fan details: Voltage :24V, Current: 0.46A rated