hi:
I use sluc610b code (EVM:UCD3138HSFBEVM-029),but The GUI was unable to find the device id in the firmware file
Could you tell me the reason and how to do for it?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi:
I use sluc610b code (EVM:UCD3138HSFBEVM-029),but The GUI was unable to find the device id in the firmware file
Could you tell me the reason and how to do for it?
Thanks.
I have never seen an issue like this with the HSFB code when it is used correctly. Just to make sure, I downloaded it from the web and compiled it and downloaded it, and I didn't see any issue.
I have made several mistakes myself in the past which have caused it to happen. They are:
1. Change the code somehow which removes the device ID from the code.
2. Try to download the wrong code
3. Try to download to the wrong device. If the code is set for the UCD3138, it can be downloaded to the 3138 and the 3138A. All other devices, like the 3138064 and 3138128 and the A versions of these devices, must be have the active version set to that device.