In production we have been using the TPS74601PBDRVR for about a couple years with no issues. Due to supply constraints, we just swapped in TPS74601PDRVR (no B) in place of TPS74601PBDRVR.
Our recent production run using TPS74601PDRVR has a very low yield (< 10%). On the failing units we do not see any output from the TPS74601PDRVR regulator; not even an aborted start. Removing TPS74601PDRVR and replacing it with TPS74601PBDRVR makes the circuit function as intended. This swap has been performed 10 times, and always fixed the problem.
The only advertised difference between the "B" and "non-B" versions of the part is the "Power-Good Rising Delay". I don't see how that difference alone can cause this issue. The PG pin is pulled up through a 10kohm resistor to the input voltage (+3.8VDC). The PG signal isn't used anywhere else in the design.
For what it's worth, the output voltage of the regulator is +3.3VDC. The EN line is pulled up to the input voltage (+3.8VDC) through a 4.7kohm resistor.
Are there any ideas on why these two parts could be behaving differently?