This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

finding a small package for negative power with 3.3~5V input / -2V/600 mA outpur current rating

Other Parts Discussed in Thread: TPS62933

Could any one suggest for small package for negative power output

input power : 2.5V ~ 5V

output power : -2V @ 600mA  at least

Thanks a lot.