Other Parts Discussed in Thread: LM5108
Hi
Electromagnetic heating was used in an HNB E-Cig project. Two heating coils are connected in series. The input voltage is 6V, and the peak operating current reaches 5A. Could you pls help recommend a suitable half bridge driver with not bad supply and small size? A competitor may be ADP3110A. Many thanks.
Regards,
Hailiang