Other Parts Discussed in Thread: TPS63060
Hello TI experts,
my customer wants to use TPS63070 for their new product.
the conditions of customer are as below;
input : 2.7V ~ 12V
output : 5V/1A or 6V/1A
I confirmed that 5V/1A is working well on WEBENCH using TPS63070, but 6V/1A is now working because junction temperature is too high.
(it was simulated up to 5.5V/1A, junction temperature was 124.751 degree at that time. please see the design report below.)
so I want to asking you that I really cannot use TPS63070 under the condition. (input:2.7V~12V / output 6V/1A)
for your information // they used TPS63060 before, it was fine under those 2 conditions.
please check this issue. Thanks.
Best regards,
Chase