This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1: Unable to fetch Authentication Key

Part Number: BQ78350-R1
Other Parts Discussed in Thread: BQSTUDIO, BQ26100, EV2400

Hi, We are using BQ78350-R1 for battery management. For testing purpose, we have connected that module to pc through EV2300. 

PC side we are using Battery Management Studio ( bqStudio ) 1.3.101. As per our requirement, we have to authenticate the battery as connected to our PCB. So to authenticate, we require default Authentication Key.

Using BQStudio, we are unable to fetch the Authentication key. So we want help, regarding this.

 

Waiting for your kindly reply

Thanks & Regards

Tapasendra Datta

  • Hi Matt Sunna,

    Thankyou for the reply,

    This link is for seal or unseal the device but we requires authentication key, so please send details regarding that, as per datasheet we are passing 0037 to Manufacturing access() but still we are not getting 16byte authentication key.

    Waiting for your kindly reply

    Thanks & Regards

    Tapasendra Datta

  • Hi Tapasendra,

    The default unseal keys are 0414 3672 and the full access keys are FFFF FFFF.

    If you have modified the keys, there is not a way to read the keys (this would not be secure since someone could read the keys you programmed). Command 0x0037 is used to program new keys, not to read the keys.

    Best regards,

    Matt

  • Hi Matt Sunna,

    Thankyou for the reply,

    Ok, but i don't want to create a new key just want to read it, to program BMS in host.

    how to read the key?

  • Command 0X0037 for Authentication Key is not accepting in 0x00 ManufacturerAccess(), Is there any way to check it through 0X44 ManufacturerBlockAccess().

  • Tapas,

    As I said before, there is not a way to read the key. The command 0x0037 is only for changing the key.

    Regards,

    Matt

  • Matt Sunna,

    please check, i'm having confusion with the bqstdio authentication technique.

    I have attached a document that mya help you

    thankyou

    For changing authentication Key and verifying authentication code.
    
    As per BQ78350-R1 Technical Reference
    17.2.32 ManufacturerAccess() 0x0037 Authentication Key
    This command enters a new authentication key into the device.
    0x0037 AuthenticationKey(): This Manufacturer Access command allows users to change the
    authentication key. Sending the new authentication key through ManufacturerBlockAccess() is
    supported. Additionally, the gauge also supports the approach of updating the authentication keys by
    sending the new keys to ManufacturerInput().
    
    Verification ( As per BQ78350-R1 Technical Reference, Page no. 75)
    1. Generate 160-bit message M using a random number generator that meets approved random number
    generators described in FIPS PUB 140–2.
    2. Generate SHA-1 input block B1 of 512 bytes (total input = 128-bit authentication key KD + 160-bit
    message M + 1 + 159 0s + 100100000).
    3. Generate SHA-1 hash HMAC1 using B1.
    4. Generate SHA-1 input block B2 of 512 bytes (total input = 128-bit authentication key KD + 160-bit hash
    HMAC1 + 1 + 159 0s + 100100000).
    5. Generate SHA-1 hash HMAC2 using B2.
    6. With no active ManufacturerInput() data waiting, write 160-bit message M to ManufacturerInput() in the
    format 0xAABBCCDDEEFFGGHHIIJJKKLLMMNNOOPPQQRRSSTT, where AA is LSB.
    7. Wait 250 ms, then read ManufacturerInput() for HMAC3.
    8. Compare host HMAC2 with device HMAC3, and if it matches, both host and device have the same key
    KD and the device is authenticated.
    
    TEST 01
    Our Authentication Key at write block 0x44= 37 00 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 01
    
    TI Battery Management Studio ( bqStudio )Version : 1.3.101 Build 1
    Input Challenge through bqstdio write block 0x2F= C8 2C A3 CA 10 DE C7 26 8E 07 0A 7C F0 D1 FE 82 20 AA D3 B8 
    Output= AD B2 D8 9D 38 F6 DF 5B 09 88 50 54 19 35 F8 4E C6 1E 0D B3 
    
    https://www.pelock.com/products/hash-calculator
    calculate using Hex String hash value
    Verificatuion
    M=C8 2C A3 CA 10 DE C7 26 8E 07 0A 7C F0 D1 FE 82 20 AA D3 B8 
    total input= 
    01000000000000000000000000000001C82CA3CA10DEC7268E070A7CF0D1FE8220AAD3B880000000000000000000000000000000000000000000000000000120
    E9A752A18D502F52CAC4BBEBD284394B4480EE9F
    01000000000000000000000000000001E9A752A18D502F52CAC4BBEBD284394B4480EE9F80000000000000000000000000000000000000000000000000000120
    FEA2347299A215DB072EF4C2524BE994AF9CFFB1
    
    Not the same...
    
    
    TEST 02
    Our Authentication Key at write block 0x44=  37 00 01 00 00 00 00 00 00 00 00 00 00 00 00 00 00 01
    
    TI Battery Management Studio
    Input Challenge through bqstdio write block 0x2F= 33 32 31 30 2F 2E 2C 2D 2B 2A 29 28 27 26 25 24 23 22 21 20 
    Output+ 60 2D F8 53 A8 09 BC 7F F9 DD BE 7C 7F B9 1C 2D 17 C2 61 ED 
    
    
    https://www.pelock.com/products/hash-calculator
    calculate using Hex String hash value
    01000000000000000000000000000001333231302f2e2c2d2b2a2928272625242322212080000000000000000000000000000000000000000000000000000120
    B386C98611DA291B7E32E85901B457A90B214071
    01000000000000000000000000000001B386C98611DA291B7E32E85901B457A90B21407180000000000000000000000000000000000000000000000000000120
    3AE076BCB7AF91617253F83C3F22F3AC3695B835
    
    Not the same...
    
    We follow this document also: "How to Implement SHA-1/HMAC Authentication for bq26100"

  • Tapas,

    I am not familiar with this document. Are you not able to unseal the device after changing the authentication key? As I said before, you cannot read the key. Please help me understand what you are trying to do.

    Thanks,

    Matt

  • Hi,

    we are able to unseal the device after changing the authentication key. Our job, programmatically we should send the 20byte message to bq78350-R1 and receive the generated SHA1 encrypted message as BMS software is doing. Now in our software also we should calculate the the same and compare with the receive one.

    In this case, we are using the generic SHA 1 code and same exercise we are doing. But the output not same. 

    So we want proper support in this SHA1 implementation.

    Referring  "BQ78350-R1 Technical Reference, Page no. 75" and "How to Implement SHA-1/HMAC Authentication for bq26100 (Rev. A)" documents. 

  • Hello Tapas,

    Just for your reference and others, there is a good E2E thread about SHA1 implementation here: https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/886762/bq28z610-faq-bq28z610-authentication-flow/3279096#3279096

    I checked with bqStudio and some other tools (Python 2 using Crypto.Hash SHA library, and online calculator) and get the same value from both using the below key and challenge:

    key =                  '01000000000000000000000000000001'
    challenge =        'C82CA3CA10DEC7268E070A7CF0D1FE8220AAD3B8'
    And the Python library:
    First full hash: 01000000000000000000000000000001C82CA3CA10DEC7268E070A7CF0D1FE8220AAD3B8
    SHA1 first digest: 676e7e3a5224fa67c45cb8cc6ce320d65703e43d
    SHA1 TI-HMAC: da9fc5d2700bd2274904b997149cd2e7ac736d53
    Padding is added using the library to the first hash input. It's very common that online tools have the wrong encoding or other small differences that can lead to calculation errors.
    Using this online calculator with Hex type I was able to get the same result: https://emn178.github.io/online-tools/sha1.html
    Sincerely,

    Wyatt Keller

  • Hi Wyatt,

    Thank you for your nice reply. Its working. Slight smile

    One more doubt I have, programmatically how to transmit block data through SPI/UART channel?  

    As we are using 2F address location for Authentication (BQ78350-R1). Now we are writing as block-write with " B8 D3 AA 20 82 FE D1 F0 7C 0A 07 8E 26 C7 DE 10 CA A3 2C C8 2F" / " 2F B8 D3 AA 20 82 FE D1 F0 7C 0A 07 8E 26 C7 DE 10 CA A3 2C C8 ". Bur not getting any data. Block read able to hndle, but block write unable to handle.

  • Hello Tapas,

    Can you clarify your question? From the example it looks like both commands were successfully sent and received. Make sure you turn off the auto refresh and do not send any other commands for 4 seconds around authentication.

    Sincerely,

    Wyatt Keller

  • Hi Wyatt,

    Actually my question on How to send Block-write command to BQ? We have made our own Power supply board (intelligent) which will talk another board (BQ chip present and third party board) through SMBus. Now requirement to authenticate the BQ device. In that case, we are writing Address and reading the data through SMBus. But for block-write, how to send? we are  not able to achieve.

    Some sample shared,  Now we are writing as block-write with " B8 D3 AA 20 82 FE D1 F0 7C 0A 07 8E 26 C7 DE 10 CA A3 2C C8 2F" / " 2F B8 D3 AA 20 82 FE D1 F0 7C 0A 07 8E 26 C7 DE 10 CA A3 2C C8 "

    Here "2F" is the address and  remaining's data.

    Regards

    Tapas 

  • Hello Tapas,

    I am still not sure I understand your end goal, it looks like the write/read blocks are being sent successfully, you should be able to use the returned block data to authenticate the gauge with your key and message. Are you saying the returned data does not match the key you programmed previously?

    Sincerely,

    Wyatt Keller

  • Hi Wyatt,

    Till date we are using pc software and writing data through EV2300 to BQ chip. Now I have to replace pc software and EV2300 with my embedded software which is running in another microcontroller. Now my embedded software will talk to BQ chip through SMBus line. With this configuration, we are writing to single address and reading the proper value. But when we want to write block (more than one byte) that time we are not receiving data. Sample block data like " B8 D3 AA 20 82 FE D1 F0 7C 0A 07 8E 26 C7 DE 10 CA A3 2C C8 2F" or " 2F B8 D3 AA 20 82 FE D1 F0 7C 0A 07 8E 26 C7 DE 10 CA A3 2C C8 " where 2F is the address, added in last or in first.

    Thanks & regards

    Tapas

  • Hello Tapas,

    The best way to confirm how your microcontroller is communicating vs the TI toolchain (EV2400 and BQStudio) is using a logic analyzer. That way you can see if you're missing a byte or something with the protocol.

    From the SMBus specification:

    http://smbus.org/specs/smbus20.pdf

    Sincerely,

    Wyatt Keller