Hi Team,
Issue:
bq24296M System Status Register REG08 - CHRG_STAT status toggling between Fast Charging and Charge Termination Done
Setup:
VIn - DC Adapter(5.0 to 5.2V)/2A
Battery type - 4.2V
ICHG - 512mA
Average System Current - 370mA(excluding battery charging)
Watchdog is disabled
SYS_MIN is set to 3.0V
Description:
bq24296M is charging normally till the battery voltage reaches 3.6V and after that the CHRG_STAT status toggling between Fast Charging and – Charge Termination Done. Battery is no more charging.
Registers Status:
Reg0 - 0x7E
Reg1 - 0x11
Reg2 - 0x00
Reg3 - 0x11
Reg4 - 0xB2
Reg5 - 0x88
Reg6 - 0x73
Reg7 - 0x4B
Reg8 - 0xA4/B4 (Toggling between 0xA4 and 0xB4)
Reg9 - 0x00
Any help is appreciated. I have gone through similar questions related to STAT toggling issue but couldn't find resolution (e2e.ti.com/.../bq24296m-stat-pin-flickering-when-battery-voltage-go-above-4v