This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54394: Min Vin1 and Vin2 voltage questions

Part Number: TPS54394

Minimum Vin1 and Vin2 for TPS54394 for output of 1.1V on VOUT1 and 3.3V on VOUT2.

I am designing this regulator with the input range of 4.5V to 16V (USB-C VBUS), and so I need the TPS54394 for output to be 1.1V on VOUT1 (worst case 600mA) and 3.3V on VOUT2 (worst case 700mA).  The min Vin is a bit confusing and I need confirmation that if I only have 4.5V on the input to both Vin1 and Vin2 that this regulator will be able to output the 3.3V and 1.1V.  Can someone verify that this is possible?

Thanks